For each package there are EDS files available, which support the applications for the iC7-Aqua Drive.
 
The latest released EDS file is backward compatible with previous versions.
 
Please note, that the information in the latest released EDS file is only supporting the corresponding released application software version. It will be possible to use the file with previous versions of the iC7-Aqua Drive, but the information in the file, can't be guaranteed to match the application software.
 
*************************************************************
 
Version history:
 
EDS_iC7-Aqua_20260303: This file is released with the release of iC7-Aqua products iC7_Aqua-2026.3.3-GR.1